STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Open keyboard when pressing on textArea?

HiIs there a solution to open a keyboard when pressing on a textArea?Now I have implemented a flexButton and a textArea above that button. By clicking on the text/button the keyboard is popping up. If you have lots of textAreas that's too much work.R...

Assertion Failed in simulator

Working on STM32F746G-Disco board, my app works on board, simulator compiles on Visual Studio, but won't compile on TouchGFX designer and keeps saying " fatal error: mvp/MVPApplication.hpp: No such file or directory #include <mvp/MVPApplication.hpp>b...

0690X00000AR8gGQAT.png
Zui by Senior
  • 814 Views
  • 0 replies
  • 0 kudos

Use LibJPEG to Decompress JPEG

Hi all,I`m trying to build a project with STM32CubeMX , Using FATFS for SDcard and Decoding JPEG with LibJPEG.And I just want to test if it can decompress successful or no,but it stacks in{ jpeg_start_decompress } function.I have no ideal about why i...

0690X00000AR8TqQAL.png 0690X00000AR8U0QAL.png

Reading JPEG & Decompress

Hi all,I`m trying to build a project with STM32CubeMX , Using FATFS for SDcard and Decoding JPEG with LibJPEG.And I just want to test if it can decompress successful or no,but it stacks in{ jpeg_start_decompress } function.I have no ideal about why i...

Errors due to windows.h

We are facing issues in compiling STemWin has windows.h headers are not found, below is the log for same. Please help us.D:/TEST/Middlewares/ST/STemWin/inc/GUI_SIM_Win32.h:52:10: fatal error: windows.h: No such file or directory #include <windows.h> ...

PSK by Associate
  • 817 Views
  • 0 replies
  • 0 kudos

Startup problem

Hello,I've built a semi-functional demo project for a client of ours using touchGFX 4.10.0 through STM32CubeIDE for a STM32F746BGT6 processor. One of the remaining issues I need to resolve has to do with the startup of touchGFX. When I flash the code...

DWeie by Associate III
  • 3888 Views
  • 8 replies
  • 0 kudos

ScrollableContainer scroll speed is not fast enough

Hi ST-Community,I already set the speed of the scrollable container to maximum via calling of the function setMaxVelocity(0xffff).But I'm still not satisfied with the actual scroll speed.is there any other possibility to increase the scroll speed?BRD...

DPfei.16 by Associate III
  • 1438 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.