STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

TouchGFX QuadPSI, Designer example vs CubeMX

I created a CubeMX Project for the STM32F746G-DISCO board.- STM32CUBEMX (5.6.0)- STM32CubeIDE (1.3.0)- TouchGFX Generator (4.13.0) I selected the board template,But the QuadSPI settings are different from the TouchGFX designer examples.Bug? or minor ...

MEder by Associate III
  • 1245 Views
  • 3 replies
  • 0 kudos

Resolved! Plans to add MAC OSX support to TouchGFX?

Hi,is there any plans to add support for MAC OSX to TouchGFX as all other ST tools seem to be multi platform? It would be greatly appreciated :smiling_face_with_smiling_eyes: Kind Regards,Steinar

SThon.1 by Associate II
  • 1421 Views
  • 1 replies
  • 0 kudos

Resolved! Dimensions cannot be changed

Thank you for helping.environmentTouchGFX Ver4.13.0STM32F769I-Discovery templateCannot change from 800 * 480 in Config-Display-Dimensions.This has been changed in 4.12.0.What should I do if I want to change the size?Thank you.

Ebun.1 by Senior
  • 1663 Views
  • 3 replies
  • 0 kudos

Resolved! DMA2S issues configurations

I am using the DMA2D in STM32F750Z8T's perform operations on buffers that are in external RAM.I am using it for drawing on the display, so I have the LTDC device active and the synchronization interrupt active.The first thing I do is fill a buffer wi...

Luca G. by Associate III
  • 978 Views
  • 1 replies
  • 0 kudos

Can't run TouchGFX designer through a samba share.

Hi,I'm a new user of TouchGfx designer. As I'm running a Linux workstation I find it inconvenient to dual boot into Windows for using this tool.So I have set up a virtual Windows guest on my Linux host.On my Linux host I have the project files and ru...

JScot.2 by Associate II
  • 3049 Views
  • 6 replies
  • 0 kudos

Resolved! modify texts.xlsx

When Microsoft excel 2016 opens texts.xlsx, it will report some error. If I accept corrections and save the file, the designer can not recognize the file.the text resource accumulates more and more, I must re-order the content. Which version or what ...

shark by Senior
  • 5075 Views
  • 12 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.