STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

DCMI with DMA on stm32743 MCU

Hullo guys , I 'm trying to get my OV10635 cam working with STM32H743 , and I have set up all required configurations , I want to get snapshot , transfer the chunk of data to internal RAM , but the FRAME interrupt is never generated , while LINE inte...

BBhoo.1 by Associate
  • 1131 Views
  • 0 replies
  • 0 kudos

Resolved! Animated image issue on custom board with 5' TFT

Hello,i used the STM32CubeIDE Version: 1.1.0 with TouchGFX designer 4.12.3 to build a project for the F746G-Disco. Everything worked fine, i was able to display animations etc.Then, i made the changes to my custom board (based on Disco schematics) to...

SKokk.1 by Associate II
  • 10944 Views
  • 27 replies
  • 0 kudos

STM32H7B3I-DK Example projects "STM32Cube_FW_H7_V1.7.0\Projects\STM32H7B3I-DK\Demonstrations\STemWin" RomLess and Xip (executable on OctoSPi).

Hello, I'm working with the STM32H7B3I-DK.I want to use this project in Romless and Xip (executable on OctoSPi).I just change the file .id (attached) , main.c (without MPU_Config()) and VECT_TAB_OSPI configuration. Problem:The pictures are not good (...

Agran.1 by Associate II
  • 1962 Views
  • 1 replies
  • 0 kudos

Why is there no 8 bpp option for GFXMMU?

My framebuffer is 8 bpp in L8 format, but under GFXMMU > LUT Configuration > Display BPP, there is no 8 bpp option? Am I missing something? Considering the LTDC supports 8 bpp framebuffers, this should definitely be an option.Currently running the la...

CBald by Associate III
  • 1958 Views
  • 4 replies
  • 0 kudos

STM32F746G-DISCO, STM32CubeIDE, TouchGFX, FreeRTOS

There is a "click" button on the screen. The status of this button is sent to the user program. There is a second "toggle" button on the screen. The first button must put the second button in a non-pressed state if it was depressed. the user program ...

AD�?b by Senior
  • 1634 Views
  • 4 replies
  • 0 kudos

How can I use an image stored in µSD ?

Hi,I want to use an image stored in µSD card.I found the following exemple : STM32Cube_FW_F7_V1.15.0\Projects\STM32746G-Discovery\Applications\Display\LTDC_PicturesFromSDCardBut it is a still image.What I want to do :Create the design with TouchGFX. ...

MMerc.1 by Senior
  • 3354 Views
  • 11 replies
  • 0 kudos

Resolved! texture mapper In the designer

Hello, everyoneWhen I adjusted the Angle in the designer, I got a lot of decimal places.why is this?I only use the buttons in the designer to adjust the Angle./korry

0693W000001prncQAA.png
Korry by Associate III
  • 1601 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.