STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! MVP Application Error

Hi ST,I have problem with MVP when applying BaseView for Views.complier said cannot convert argument 1 from 'PresenterType' to 'T &'Please help me fix the problemThank you.

HNguy.21 by Associate II
  • 2153 Views
  • 4 replies
  • 0 kudos

ScrollWheelWithSelectionStyle resize at runtime

I have a ScrollWheelWithSelectionStyle instanciated from the designer, so it is placed inside the ViewBase, with a certain size.What I whant is to be able to resize it in height from the View. This is because when instanciated it is set to hold 4 ele...

LRaim.1 by Associate
  • 1851 Views
  • 3 replies
  • 0 kudos

Enviroment run simulation

Hi ST,I want to send out package debug/bin to show demo on simulate. How to run this simulate if don't install visual studio and touchgfx? what file should include to this package?Thanks

NHo.1 by Associate III
  • 1520 Views
  • 3 replies
  • 1 kudos

Resolved! What is handleTickEvent() period?

Hi,This is the code snippet to animate containerAF1:void mainScreenView::handleTickEvent() { static uint32_t startMove = 0; startMove++; bool pr; if(startMove<40) pr = true; else pr = false; containerAF1.setVisible(pr); containerAF1.invalidate(); if(...

RGajd.1 by Associate II
  • 2128 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.