STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Keil and touchGFX broken

I'm new to touchGFX and I'm using Keil (v5.xx). I cant compile the touchGFX example for the 746G-Discovery due to missing files and I'm having the same kind of problems when I generate a project using the designer.When I try to compile the example (S...

allard by Senior
  • 1962 Views
  • 3 replies
  • 0 kudos

Drawbitmap/ GUI issue in Free RTOS

Hi,STM32F429iiI couldn't load image or draw any pattern from different tasks. If I load a bootup image from default task (TASK1), and switch over to another task and try to clear the bootup image and draw my own lines and patterns. But the boot up im...

High efficiency method of side mixing and side display

Due to THE MCU's RAM and ROM limitations, I wanted to use the pre-stored 4bit bitmap data to mix the 16-bit color and display as I mixed.The current method is to use GUI_DrawPixel() every time the color is mixed in the control's custom redraw functio...

lxw by Senior
  • 695 Views
  • 0 replies
  • 0 kudos

Resolved! Added a Graph Widget but nothing is shown on the display

I downloaded GraphApplication from this post to try Graph Widget. https://community.st.com/s/question/0D50X0000ALvsTfSQJ/how-to-start-using-the-graph-widget-from-touchgfxopenrepository-in-touchgfx-designerI am using STM32F429i-Discovery Board to disp...

0693W000003BI5hQAG.png 0693W000003BI5wQAG.png
HPam.1 by Associate II
  • 1814 Views
  • 3 replies
  • 0 kudos

STM32H747 discovery kit

I have a question about the LCD BD in the STM32H747 discovery kit.B-LCD40-DSI1I'd like to know exactly what LCD is in the above product (whether it's frida or KJD) and if there's a data sheet that gives me accurate information about LCD BD Dimension....

YAn.1 by Associate
  • 752 Views
  • 0 replies
  • 1 kudos

Resolved! Compilation error due to "using namespace"

When the designer generates the code for a screen (file "XXXViewBase.cpp") containing a widget with a wildcard, it generates code like this:txtCount.setPosition(301, 94, 152, 89); txtCount.setColor(touchgfx::Color::getColorFrom24BitRGB(255, 255, 255)...

SZano by Associate III
  • 1469 Views
  • 1 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.