STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STM32L073 LCD Flags FCRSF and RDY flag not set

Hello, I've a smal implementation for the STM32L073 without using of the HAL. For the configuration of the LCD peripheral the flags FCSRF and RDY not set.I see that the flag FCSRF is reset during writing new values in the register FCR. The MCU have t...

bm2 by Associate III
  • 971 Views
  • 0 replies
  • 0 kudos

Two task in touch gfx

Hi, I'm using FreeRtos v1 , my board is stm32f429... . I have to thread in main.c and I generate them by stm32cubemx ...in one thread I have a touchgfx process . Other is a task for ethernet . Both of them have a same priority and the stack size of t...

S_bgh99 by Associate III
  • 1941 Views
  • 3 replies
  • 0 kudos

Inverting colors

Hello, I have a 1bpp display and would like to invert the colors on all screens programatically. I've tried in a) getColorFrom24BitRGB(uint8_t red, uint8_t green, uint8_t blue) by XORing with 1, which is ok except for bitmapsb) TouchGFXHAL::flushFra...

Using a Touchscreen with Stemwin.

Hello all. I am using an STM3220G-EVAL board with 3.2" TFT and resistive touchscreen. I am using STEMWIN and would like to use the touchscreen. Can anyone point me in the direction of examples of using touch controller with this particular graphics l...

defacato by Associate II
  • 1323 Views
  • 1 replies
  • 0 kudos

Resolved! Dynamic bitmap in background

Hello,I used the following article to have a dynamic bitmap on the screen:https://touchgfx.zendesk.com/hc/en-us/articles/207460605-Dynamic-Bitmaps-Load-images-at-runtimeThen I draw a screen in touchgfx designer (attached designer.jpeg) where I would ...

DVale by Associate II
  • 6155 Views
  • 6 replies
  • 0 kudos

image binary to sd card

hi, i have a little problem. i'm using stm32f4 and i want to run touchgfx. i generate code and i copy image to an array then i wrote array in binary format... all thing is good but when array size increase . i have below error.Not enough information...

S_bgh99 by Associate III
  • 1226 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.