STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

ScrollWheel problems

Hi,Is this the right place for bug reports? I stumbled upon some problems with the ScrollWheel widget.ScrollWheelWithSelectionStyle::setSelecteItemOffset is misspelled and is not overriding the intended setSelectedItemOffset. Unless I have done somet...

Ansa by Associate
  • 2320 Views
  • 6 replies
  • 0 kudos

3.5" LCD (320x480) & MCU Interface

I am trying to use a 320x480 TFT LCD with the STM32F767IIT, FreeRTOS, TouchGFX.I think that the 450 Kbytes (320xRGBx480) capacity is required, but the RAM capacity of STM32F767IIT seems to be insufficient. .Any advice on whether to add SDRAM on the S...

pabian by Associate III
  • 1083 Views
  • 1 replies
  • 0 kudos

Bug in ItemSelectedCallback of ScrollList

The version of touchGFX Designer is 4.13.0.I use the function "setItemSelectedCallback" of ScrollList .ScrollList have 5 items. And display mode is no circular.In callback fucntion "scrollList1ItemSelectedHandler". When I click the item one by one, a...

Wrend.1 by Senior
  • 682 Views
  • 1 replies
  • 0 kudos

Resolved! [ ToucgGFX ] Issue when display string in TextArea

Hello, I'm trying to display a random String in TextArea.But when I call this function, there is too much ???? was displayed.Below is my code, anyone can tell me what's wrong?Many thanks, Hieu const char * test = "Hello World"; Unicode::snprintf(Roo...

0693W000003RxaiQAC.png

Resolved! Firmware crashes with dynamicBitmap in TouchGFX

I'm using TouchGFX's dynamicBitmaps to load an image that I have in a buffer.The problem is that, even just using the example I found at this link https://support.touchgfx.com/docs/development/ui-development/touchgfx-engine-features/dynamic-bitmaps:B...

0693W000003Rl5nQAC.png
Luca G. by Associate III
  • 1963 Views
  • 3 replies
  • 0 kudos

Resolved! [TouchGFX]The effect of "change screen" function in PC simulation and development board is not consistent

I add a function like "application().gotoScreen_startScreenSlideTransitionWest();"It works well in PC​ simulation,but it works in real board like the "application().gotoScreen_startScreenNoTransition".Maybe it need some setup to make it works in ​dev...

Wrend.1 by Senior
  • 2082 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.