STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Can I make a global warning window?

I want to display a ​warning window when a single triggered from hardware.It seems that if I want to achieve this effect in touchGFX, I need to add a model window to each interface. Can I add a global window to implement it elegantly?:face_without_mo...

Wrend.1 by Senior
  • 1708 Views
  • 2 replies
  • 2 kudos

Resolved! SDRAM capacity used by Touch GFX

Thank you for helping.How much SDRAM capacity does TouchGFX actually consume?Please tell me the unit in bytes.environmentboard: STM32F769I-DISCOTouchGFX: Ver4.15.0

Ebun.1 by Senior
  • 1568 Views
  • 2 replies
  • 0 kudos

How to work with pixels?

Hello!I put to project a widget box1, it's color is white.I want to set color of each pixel of boxlike this: SetPixel(x,y, R,G,B);And after I want to read color of pixel? like this: color=GetPixel(x,y);How can I do it in TouchGFX?

EEuge by Senior
  • 1525 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F746G-DISCO, TouchGFX

Hi Problem. There are two screens, S1 and S2. The S1 has two buttons. GO to change screen to S2 and ON to set output pin. The ON button state is sent to main.c. I want to change the screen after pressing GO, but also the state of the ON button. How t...

AD�?b by Senior
  • 1516 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.