STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

TouchGFX Using SPI with STM32H7

Hey There,I am working on a project that will involve using a STM32H743VIT6. Its quite a complex board so almost all of the pins one the MCU have been occupied. Because of this I have to drive the 240x320 LCD-TFT with SPI ( Driver is ILI9341). I was...

RThom.5 by Associate
  • 974 Views
  • 0 replies
  • 0 kudos

Resolved! Is there an alternative to ButtonWithLabel in Touchgfx?

I am using TouchGFX ButtonWithLabel widget to have text within my buttons. It requires Resource texts and the function setLabelText() has TypedText as an argument. I want to replace the label with my own custom string which can change during runtime ...

TLe.4 by Associate II
  • 1184 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F469 discovery, black screen

Hi, I Have recently uploaded a simple Led Blink code on my STM32F469, since that the screen is always black and doesn't show anything.I want to know how to go back to the default code that was on this board in order to make the screen work normally a...

STM32F469 Weird Half-Executing old program stuck

I'm still struggling to get STM32F469 to run TouchGFX. Something REALLY weird happened yesterday, and I wasn't able to recover Disco board since.I have 2 projects in STM32CubeIDE:Project 1 turns on the screen and has some GUI - I backed up that proje...

ilyus by Senior II
  • 3093 Views
  • 6 replies
  • 0 kudos

How to make SlideMenu swipeable?

Hello, is there a way to make the SlideMenu Container swipeable, reacting not only on the stateChange button, which starts the animation, but also on a swipe an move to to the current position of the touch. The idea is to make a slidemenu behaving li...

SKowa.1 by Associate
  • 1191 Views
  • 1 replies
  • 0 kudos

L8_RGB565 images issue

Hello,To save space on the section "ExtFlashSection" with the dev board STM32F469I-DISCO, I'm trying to use the L8_RGB565 format for my backgrounds. I'm doing this by changing the "Image Format" of all background on the "Images" section of TouchGFX D...

0693W00000ANZGtQAP.png 0693W00000ANZHwQAP.png
TDele.1 by Associate III
  • 3676 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.