STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STM32H7B Workshop 2020

Unzip full codePage 49 of PDF• Unzip the STM32H7B3Workshop2020_modified_files.7z tothe C:\2020_ST_GFX_WS\STM32H7BWorkshop2020• It will overwrite the existing files with the implementation for all labs withinpre-processor directives #ifdef• The modifi...

AClin.2 by Associate
  • 1803 Views
  • 3 replies
  • 0 kudos

Storing TouchGFX images in SD Card

Hello everyone,I am successfully developing a project on an STM32F469I-Disco. The chip is starting to lack space so I am looking into storing TouchGFX images on an SD Card. I am almost successfully using my SD Card to write and read data. I also chec...

NKieg.1 by Associate III
  • 1812 Views
  • 2 replies
  • 2 kudos

We are using the OSPI port of STM32L4P to communicate with the DCMI port of STM32F427, and the problem is the end of data signal was sent, but there is no interrupt from the DCMI, while if we reset the OSPI of STM32L4P, the interrupt appears.

We are using the OSPI port of STM32L4P to communicate with the DCMI port of STM32F427, and the problem is the end of data signal was sent, but there is no interrupt from the DCMI, while if we reset the OSPI of STM32L4P, the interrupt appears.

mchen.1 by Associate
  • 1063 Views
  • 1 replies
  • 0 kudos

How to show animation?

Hi,Now I am thinking about adding animations when screen startup and normal screen , is there any implement in touchgfx? If not, I want to know if it is feasible to decode images from some format like GIF and just show them by order to realize this?...

JJ.Lin by Associate III
  • 980 Views
  • 1 replies
  • 0 kudos

STM32 UART TouchGFX 4.17.0

Hi,I am working on TouchGFX for STM32H747 Discovery Kit. I get this error when i try to add a UART to my project. Please let me know.Thank you,Enes Ozkaya

Enszky by Associate
  • 1884 Views
  • 1 replies
  • 0 kudos

Any sample code how to detect gesture event?

Hi I want to detect gesture event like swiping to left and right without using the Swipe container.Any sample code for this?The usage is, I have a container which would behave differently when:Single clickLong press swipeI can do 1 and 2, but now I n...

BParh.1 by Senior III
  • 936 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.