STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

TouchGFX Invalidate causes CFSR_UNALIGNED

Call to MainView::invalidate for a text box causes CFSR_UNALIGNED inside TouchGFX function, in vicinity of TextProvider::endOfString.Have commented-out our code change to text box text, and simply call invalidate, and observe crash.Tried solutions 1 ...

Can I control Micro OLED display without special drivers or controllers over SPI or I2Cjust using the embedded LCTD controller.

Hello,I didn't found any answers for this so I would like to know if I can control micro oled display (high resolution, small density oled, 0.23", VGA res. or something little bit higher) in my smart glasses using some of STM 32 bit MCUs, ik external...

Partial Frame Buffer (4.15) maximum transmitted lines

I'm using partial frame buffers with CubeIDE 1.5.0 and TouchGFX 4.15. I've found that when updating large portions of the screen, the function touchgfxDisplayDriverTransmitBlock is never called with a height larger than 20 lines, regardless of the fr...

ebray by Associate II
  • 2542 Views
  • 3 replies
  • 0 kudos

Why the CubeIDE can't generate an STM32H747 based project, and why can't generate the TouchGFX also the GUI? (STM32CubeIDE 1.7.0; TouchGFX 4.0.17)

Hi guys,I want to develop a project, for which needs a display, and i chose the TouchGFX way. I'm using the STM32H747 microcontroller. In TouchGFX exists demos for STM32H747I Disco board, but my application will run on a custom designed board.So I tr...

For touchGFX application, I have created a project for implementing touchGFX(STM32F411RE) with external SPI flash memory(W25Q32) but I am facing a problem in programming the chip with an external loader but the external loader working well in using as alo

19:47:11 : STM32CubeProgrammer API v2.5.019:47:17 : ST-LINK SN : 0670FF53515587828114321419:47:17 : ST-LINK FW : V2J38M2719:47:17 : Board : NUCLEO-F091RC19:47:17 : Voltage : 0.02V19:47:17 : SWD freq : 4000 KHz19:47:17 : Connect mode: Under Reset19:47...

DCMI or DMA problem. Detecting end of capture

Hello,I am facing strange problem. I have a camera that transfers data, 90kPixels.Since it is 10 bit camera, and data is packed into 32b word, I can tranfare image in singe DMA config ((300x300)/2 in DMA)So I have Circular DMA buffer, continuous DCMI...

Linas L by Senior II
  • 1896 Views
  • 2 replies
  • 0 kudos

Importing Typographies

Hi,I want to use a TextLabel container found in another project.I manually edited the Designer's .touchgfx file and copied the relevant cpp/hpp files.Unfortunately, this class assume the presence of about 30 typographies and resources, which are of c...

CHech.1 by Associate III
  • 795 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.