STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

touchgfx stm32f746 framebuffer issue.

Hi,I am using a custom lcd 800x480 on stm32f746 disco, with touchgfx.The project is generated by cubeMX ( Freertos , FMC 16bit, LTDC RGB565 one layer) and modified with lcd parameters.Static images are printed OK on lcd, but when any widget moves, in...

IDim.1 by Associate II
  • 815 Views
  • 0 replies
  • 0 kudos

stm32f746 disco +touchgfx+ custom 800x480 LCD

Hi,I am trying to integrate an 24-BIT parallel LCD RVT50HQTNWN00 with stm32f746disco board.Code was initially exported from touchgfx designer 4.18.0. for the disco board and then edited in cubemx. original 480x272 was removed and the new lcd was sold...

0693W00000GZ991QAD.png 0693W00000GZ98rQAD.png 0693W00000GZ98mQAD.png 0693W00000GZ98cQAD.png
IDim.1 by Associate II
  • 2566 Views
  • 5 replies
  • 0 kudos

5"-7" LCD TFT screen

Hello,I want to drive 5"-7" LCD TFT screens. Do you have a suitable integration where I can do this? What do you think I should use? I will do mass production. I am waiting for your good integrated suggestions to avoid stock shortages and get quick r...

Ygndz.1 by Associate
  • 723 Views
  • 0 replies
  • 0 kudos

Resolved! Touchgfx bulleted text list?

I have an application where there is a potential for lots of text. It would be nice to break up the next into a bulleted list or a numbered list. Is there a clever way to do this with the Touchgfx framework? I think making typed text values for ea...

CPaye.1 by Associate III
  • 1404 Views
  • 2 replies
  • 0 kudos

How to configure external Sdram to avoid "`TouchGFX_Framebuffer' will not fit in region `RAM'" problem

I'm trying to build application on my custom STM32F429IITX board (no OS), external sdram is ISSI- IS42S16400J-7TL, 480x272 display, when I try to build app ,I'm getting some errors as you see below FirstProject.elf section `TouchGFX_Framebuffer' will...

0693W00000HpFlvQAF.png 0693W00000HpFZkQAN.png 0693W00000HpFZBQA3.png 0693W00000HpFmZQAV.png
Uusta.1 by Associate III
  • 3180 Views
  • 1 replies
  • 0 kudos

TouchGFX video in standalone project

I'm working on a project using TouchGFX 4.18.1 on a STM32H750VB MCU.As it's a corporate project, I use an internal framework/platform that works fine with TouchGFX 4.18.1, on IAR Workbench in addition of TouchGFX Designer.Now I'm trying to integrate ...

BDELI.2 by Associate II
  • 722 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.