STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STM32H743I-EVAL + LCD(800x480)

Hi, I want to integrate an 24-bit parallel LCD(change from 640×480 to 800×480) with STM32H743I-EVAL board. But I am a beginner for this field. So I followed this video > https://www.youtube.com/watch?v=yiHjOH7zJP0.What I have done is below:Created th...

0693W00000LyDHiQAN.png 0693W00000LyDHnQAN.png 0693W00000LyDHsQAN.png 0693W00000LyDI2QAN.jpg
BMunk.1 by Associate II
  • 2095 Views
  • 4 replies
  • 0 kudos

Problem with wildcard in textarea..

Hello everybody,i create a project using TouchGFX 4.18 to read temperature.When a button is pressed i create a routine that read temperature from a sensor and show this in a text area inside a container.In TouchGFX i create a wildcard in texarea with...

EMir.1 by Associate II
  • 2669 Views
  • 2 replies
  • 0 kudos

Detecting a page change on Swipe Container.

I am currently using a swipe container that goes between 3 pages by either swiping or using a next/back button on the bottom corners of the screen to change pages. The page indicators are overlapping with the next/back buttons when I do swiping so I ...

ALew.1 by Associate
  • 2090 Views
  • 2 replies
  • 0 kudos

How to change path to STM32CubeProgrammer

Hello folks,how and where can I change the path to the STM32CubeProgrammer in TouchGFX Designer?After hitting the Run Target Button (F6) the TouchGFX Designer fails downloading the flash file due to not find STM32_Programmer_CLI.exe.This is because t...

0693W00000D0aoiQAB.png
LBart.1 by Associate
  • 3339 Views
  • 1 replies
  • 0 kudos

The swipe GUI show delay.

I download code on MCU internal rom swipe GUI show is good(video : Ok.zip ).But I download code on external QSPI flash swipe GUI show is delay (video : Bad.zip).QSPI flash work clock on 100MHz.Why code on external QSPI flash can not work good like MC...

0693W00000LxnV0QAJ.png
YCF.1 by Associate III
  • 3070 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.