STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Change screen orientation dynamicaly

Hi,In the device we are designing, we would like to change the orientation of the screen depending on the actual orientation of the device as detected by the accelerometer. I have read the TouchGFX documentation and many posts on this forum and proce...

ypiotrp by Senior
  • 2220 Views
  • 1 replies
  • 0 kudos

Resolved! error: 'blendL8CLUT' was not declared in this scope

I have upgraded Touchgfx designer to latest version 4.21.4 .I created a new project and in the screen added a new line progress bar.I encountered linker errors c:\st\stm32cubeide_1.10.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-...

KNara.2 by Associate III
  • 2283 Views
  • 2 replies
  • 1 kudos

Issue : Sometime, the screen freezes on wakeup. The system is still running but touchgfx does not render frame anymore. Description : MCU : STM32L4R9AI with freertos and touchgfx Screen : DSI AMOLED. Drivers used : GFXMMU, LTDC, DMA2D, DSI

Test 1 conditions (freeze issue) :We want to stay active for 10s and go to into sleep mode for 10s in a loop using RTC wakeup. In the app, one task runs touchgfx and another handle the timeout to go to sleep.The condition to go to sleep is that the t...

MDod.1 by Associate
  • 1393 Views
  • 0 replies
  • 0 kudos

Resolved! QSPI

What to do if I do not want to load my images to QSPI flash every time I upload the code?

heyo by Senior
  • 2328 Views
  • 3 replies
  • 3 kudos

Error Linking Project with TouchGFX Designer

Dear ST Support Team,I am writing to report a bug that I have encountered while using the STM32U585 microcontroller with FMC communication, the ST7789v LCD, IAR 8.50.9, and TouchGFX Designer v4.21.3.I have successfully ported the virtual API stack of...

RMAST.1 by Associate
  • 1612 Views
  • 1 replies
  • 0 kudos

Resolved! Gauge Needle non appare

Hi,I make a project with touchGFX Designer 4.21.1, I place a gauge but the display show only the indicator without needle.I try with a default indicator in library.with simulator is currect. screenViewBase::screenViewBase(){   __background.setPositi...

PZamb.2 by Associate III
  • 1371 Views
  • 1 replies
  • 0 kudos

Image Rendering Problen

I had a 3.5inch display with stm32G01CET.I had design some UI with many component in it.But it had only an image which the size about 400px x 200px is incomplete rendering.So I have no idea how do I fix it

_legacyfs_online_stmicro_images_0693W00000dDSbqQAG.png
Tinnagit by Senior II
  • 1264 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.