STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Pre flashed firmware in STM32U575ZI-NUCLEO-AZ2

Hi,I want to get the access to the default pre flashed firmware image flashed while receiving STM32U575ZI-NUCLEO-AZ2 eval board. Can you share that whole firmware project along with the source code? Also, whether the UI is built using TouchGFX? If ye...

mdalal by Associate III
  • 1471 Views
  • 5 replies
  • 1 kudos

Resolved! Understanding buttons state

Hello, I just noticed that foceState and getState (for toggleButton) are not what i thought they were, until now I used to think that forceState would just simulate the press of a button for being able to press a button from the code, without physica...

Resolved! Orphaned TouchGFXDesigner processes

Process Explorer is showing a number of TouchGFXDesigner processes as running even though all instances of it have been closed (there are no windows visible).I found this when I tried to delete and folder and that failed with an "in use" message - Re...

CTapp.1 by Senior III
  • 2167 Views
  • 4 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.