2022-11-27 9:33 PM
Hi,
Why CubeMX forces the TouchGFX generator to the M4 context? I can't uncheck the M4 and assign it to M7 context from within CubeMX. I was wondering if I did something wrong or if this was known issue when generating project with TouchGFX using CubeMX?
Zaher
2022-11-27 9:37 PM
2022-11-28 5:27 PM
** Update **
It seems TouchGFX Designer has witnessed a whole lot of improvements since last time I used it. The code generated from TouchGFX has the project template I was looking for. It has included all of the following items:
This is marvelous. Such a harmony and cohesion among the tools used to generate the code is what I call a great investment and a step forward from STMicroelectronics.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.