2019-06-27 12:11 AM
I'm looking for a project with H750 that generates code for CubeMx and Keil, anyone managed to do that?
Thanks
Stefano.
2019-06-28 1:05 AM
Hi @Zui,
Just to be sure. Are you referring to Keil?
Best regards,
Martin
2019-06-28 1:14 AM
oh Gosh what did i wrote? must have been very tired, yeah, was keil, sorry
2019-06-28 1:29 AM
Haha, i figured! I just had to be sure, sorry. Maybe it was some codename for some IP :)
Okay, back to the subject. We have an application template for the H750 from the Designer, but... H7 is not available in CubeMX just yet. We are working on that and it may be supported in 5.4 of CubeMX - When that happens we'll update the ATs to support an .ioc file.
So, to be more concise - It's not supported yet, but it will be. H7 support is not ready for TouchGFX in CubeMX.
/Martin
2019-06-28 1:37 AM
any prevision for release date? Because my company needs to present a prototype for september, and we were aiming to use H750.
2019-06-30 1:19 PM
We're hoping to get H7 support in CubeMX 5.4 which would be before september, but i'm not sure how much time you'd have if you wait for CubeMX support.
The H750 Application template is already available through the TouchGFX designer. You could get a head start.
/Martin
2019-06-30 1:20 PM
Once H750 support is available through CubeMX you would just import your TouchGFX gui to an application based on CubeMX instead,
/Martin
2019-07-02 2:19 AM
Just to be more precise - You can still use TouchGFX and H7 together. We have an application template for the H750 available from the designer. It's just that TouchGFX support is not ready from within CubeMX just yet. Perhaps in 5,4.
/Martin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.