2025-09-28 7:43 PM
I'm currently using Touchgfx after updating from version 4.25 to 4.26.
When I build and run the code generated by Touchgfx 4.26, Display color doesn't match the design in Touchgfx 4.26.
But When I do the same thing through Touchgfx 4.25, Display color matched very well.
Solved! Go to Solution.
2026-01-27 8:57 PM
Sorry I am late. I solved it already..
But I forgot how to solve..Maybe I changed the RGB color setting in CubeMX.
I think It was a collision between touchgfx old version and touchgfx new version.
I saw new version's updated list on touchgfx official website.
2025-09-29 1:27 AM
Hello @MJKIM ,
Could you give more info about your application?
BR,
2026-01-27 1:18 AM - edited 2026-01-27 1:20 AM
Hey, was this ever solved?
I've run into the same problem and even with GIT Control, and reverting to a previous version I knew definitely worked. Something with the IDE or/and TouchGFX is making the colours change after updating version.
Resorting back to a previous version of TouchGFX 4.25 and colours are still in a different state
Kind regards,
Andrew
2026-01-27 1:20 AM
Have you tried deleting all generated code and generating it again?
2026-01-27 1:22 AM
Is that generated code both under TouchGFX and under STM32CubeIDE debug and application?
Thank you
2026-01-27 5:24 AM
I meant TouchGFX generated code. But you can also try STM32CubeMX code. Middlewares might not be updated.
Debug folder has no generated code, only build artifacts.
2026-01-27 8:57 PM
Sorry I am late. I solved it already..
But I forgot how to solve..Maybe I changed the RGB color setting in CubeMX.
I think It was a collision between touchgfx old version and touchgfx new version.
I saw new version's updated list on touchgfx official website.
2026-01-29 1:36 AM
Hey,
would you be able to find out which RGB color setting you changed?
Kind regards,
Andrew A
2026-01-29 4:20 PM
Is default Touchgfx setting "RGB565"?
you can check it in CubeMX.
If it's ritght, Choose another option.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.