2020-06-13 6:55 AM
hi every one.
I want to display the amount of ADC on the LCD. How can I show a variable value of ADC1ConvertedValue?
now I can only display a character on LCD.
i want to show: The ADC value is: (amount of the ADC Value)
int main(int argc, char* argv[])
{
ADC1ConvertedValue = ADC_GetConversionValue(ADC1);
char Satz1[] = "ADC1ConvertedValue";
char Satz2[] = "Hello ";
char Satz3[] = "This is a Test";
char Satz4[] = "Navid";
config_pin();
config_ADC();
lcd_init();
TIM3_Init();
lcd_set_font(FONT_FIXED_8, NORMAL_SIZE);
lcd_moveto_xy(0, 0);
lcd_put_string_length(FONT_FIXED_8, NORMAL_SIZE, &Satz1[0], sizeof(Satz1));
lcd_moveto_xy(2, 0);
lcd_put_string_length(FONT_FIXED_16, NORMAL_SIZE, &Satz2[0], sizeof(Satz2));
lcd_moveto_xy(4, 4);
lcd_put_string_length(FONT_FIXED_16, NORMAL_SIZE, &Satz3[0], sizeof(Satz3));
lcd_moveto_xy(7, 0);
lcd_put_string_length(FONT_FIXED_8, NORMAL_SIZE, &Satz4[0], sizeof(Satz4));
2020-06-13 7:23 AM
You need to convert it to a string, then you print that string. sprintf can do the converting.
> lcd_put_string_length(FONT_FIXED_8, NORMAL_SIZE, &Satz1[0], sizeof(Satz1));
The length of the string is strlen(Satz1), not sizeof(Satz1). It may work in this instance, but only if trying to print a null character does nothing.
2020-06-13 10:47 AM
Thanks a lot. I did as you said, but the LCD doesn't show anything at all. the LCD is on, but all words
int main(int argc, char* argv[])
{
char str[16];
sprintf(str,"%d",ADC_GetConversionValue(0));
char Satz1[] = "ADC1ConvertedValue";
char Satz2[] = "Herr Dr. ";
char Satz3[] = "navid ";
char Satz4[] = "Uni ";
config_pin();
config_ADC();
lcd_init();
TIM3_Init();
lcd_set_font(FONT_FIXED_8, NORMAL_SIZE);
lcd_moveto_xy(0, 0);
lcd_put_string_length(FONT_FIXED_8, NORMAL_SIZE,&str[0], strlen(str));
lcd_moveto_xy(2, 0);
lcd_put_string_length(FONT_FIXED_16, NORMAL_SIZE, &Satz2[0], strlen(Satz2));
lcd_moveto_xy(4, 4);
lcd_put_string_length(FONT_FIXED_16, NORMAL_SIZE, &Satz3[0], strlen(Satz3));
lcd_moveto_xy(7, 0);
lcd_put_string_length(FONT_FIXED_8, NORMAL_SIZE, &Satz4[0], strlen(Satz4));are deleted.
2020-06-13 11:08 AM
So if you try to display the string "1234" you only see the character "1" on the LCD? That's a different issue than just displaying a number. Maybe I misunderstood the question.
I'm not familiar with the LCD library you're using. Likely the issue is in lcd_put_string_length somewhere. Not sure I want to dive into it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.