2020-08-06 4:33 AM
2020-08-06 5:50 AM
Hi,
I am unsure I understand fully what you are trying to do but I would advise working around the handleTickEvent function . One second is around 60 ticks (this can be impacted by your UI if you have complex animations or your hardware) so you can code a delay event.
/Romain
2020-08-06 6:06 AM
When we use swipe container then container will be slide left to right or Right to left by touch event or we use Run simulator then it will slide by mouse.
swipe container does not have any callaback function or any container key who give us container slide number.
So,due to this issue I can not move 1 container slide to another slide (or any) by code.
So,I want to create function container in Screen1View.cpp who slide 1-2-3 or 1-3-2 like this and it will display like slide show (1sec interval).
2020-08-06 7:48 AM
Hello,
Indeed one thing you can do is call setSelectedPage(uint8_t pageIndex) but it will not perform the slide animation.
Look at the Scroll Wheel widget, you have the function animateToItem() that allows you to create a slide show.
/Alexandre
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.