2022-09-24 3:45 AM
Hi
I have downloaded en.x-cube-aws_v2-0-0.zip file. Imported STM32CubeExpansion_Cloud_AWS_V2.0.0\Projects\B-L4S5I-IOT01A\Applications\Cloud\aws_demos project in to STMCube IDE.(Version: 1.10.1)
I am able to build B-L4S5I-IOT01_2_Images_SBSFU and B-L4S5I-IOT01_2_Images_SECoreBin projects without any issues.
But the B-L4S5I-IOT01_aws_demos build fails with the following errors -
Description Resource Path Location Type
cannot use executable file '../../../../BootLoader_STSAFE/2_Images_SBSFU/STM32CubeIDE/B-L4S5I-IOT01_2_Images_SBSFU/Debug\se_interface_app.o' as input to a link B-L4S5I-IOT01_aws_demos C/C++ Problem
Is anyone facing a similar issue? any pointer to download AWS demo application for b-l4s5i-iot01a IoT eval board
Regards
Dhanya
2022-09-26 3:24 AM
Hello @Dhanyakumar Hosamane,
Check your setting in Properties.
Have a look at this post here: Issue building SBSFU with latest STM32CubeIDE 1.9.0 : here is the solution.
I hope this helps !
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Imen
2023-04-17 3:33 AM
@Imen DAHMEN I am facing build issues with B-L4S5I-IOT01_2_Images_SECoreBin package as
can't remove '../..\..\Inc\kms_platf_objects_config.h.tmp': No such file or directory.
Could you please specify which version of package should be considered. I am working on
2023-04-17 10:12 AM
Check your include path.
Go to Project options ->C/C++ tab->Include paths and add new paths to the include directories.
2023-09-05 1:10 AM
Maybe we've already solved it, but,
I have experience facing a similar problem.
I recommend lowering the CUBE IDE version.
In my case, I used the 1.5.0 version and it worked out
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.