2020-12-02 8:37 AM
Is it a problem if I join the meeting at 9:00? Before I have to take the children to school
2020-12-02 8:46 AM
Hello,
we usually start at 9.00 am. We connected at 8.30 to address any installation issue.
If you already done the homework, you will face no issue to follow.
Best regards,
Frantz
2020-12-02 9:07 AM
Perfect, the installation is completed without problems
See you tomorrow at 9:00
Have I to use the Microsoft Teams link? Right?
Best regards
Gian
2020-12-02 9:10 AM
Installation ok but there is two homeworks also ;)
And to connect, you just need to use the Microsoft Team link you received in the invitation.
Talk to you tomorrow !
Best regards,
Frantz
2020-12-02 9:51 AM
homeworks Just done too without problems
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.