2024-05-21 11:47 PM - last edited on 2024-07-08 7:13 AM by Peter BENSCH
Hello,
I am using the STSAFE-A110 connected to the ESP32C3 board. I referred to the service interface from this GitHub repository (https://github.com/kmwebnet/stsafe_esp32_test). I have matched the Host MAC key and cipher key exactly as in the example. The current status is that pairing is complete, and the wrap operation returns a success response. However, I am encountering a 0x11 error during the unwrap operation.
Unwrap_Failed : 17 <- print decimal data
Solved! Go to Solution.
2024-06-26 12:25 AM
Hi @Benjamin BARATTE ,
After posting the question, I checked the code and found that the CRC algorithm was incorrect. After making the corrections, I tested it and it worked.
Thank you.
Best Regards,
Darzento
2024-06-21 6:37 AM
Hi @darzento ,
As the wrap envelop is working fine, one reason to get such error is that the envelop you hare sending to the unwrap command is corrupted.
Could you check the input parameter you pass to the StSafeA_Unwrap() API ?
Best Regards,
Benjamin
2024-06-26 12:25 AM
Hi @Benjamin BARATTE ,
After posting the question, I checked the code and found that the CRC algorithm was incorrect. After making the corrections, I tested it and it worked.
Thank you.
Best Regards,
Darzento
2024-06-26 1:09 AM
Hi @darzento ,
Thanks for the feedback.
Normally, in case of CRC error in the CRC bytes, you should get a STSAFEA_COMMUNICATION_ERROR from the STSAFE-A.
Best Regards,
Benjamin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.