cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeN6: Why no CubeIDE project for Template_Isolation_XIP and Template_Isolation_LRUN?

jrocher-althea
Associate

Hello,

I am currently working with the STM32CubeN6 MCU Package and I noticed something surprising:

  • For  NUCLEO-N657X0-Q templates like Template_FSBL_LRUN and Template_FSBL_XIP, STM32CubeIDE projects are provided directly (under /STM32CubeIDE/).

  • For Template_Isolation_XIP and Template_Isolation_LRUN, however, only the ExtMemLoader project is provided for STM32CubeIDE.
    The main sub-projects (FSBL, AppliSecure, and AppliNonSecure) are only available as source files, and not as ready-to-import STM32CubeIDE projects.

This is different from the Keil (MDK-ARM) and IAR (EWARM) folders, where full projects are available for all parts.

Why are the STM32CubeIDE projects missing for the main FSBL, Secure, and NonSecure applications?
Is it planned to provide full STM32CubeIDE projects for these templates in a future update?
Or is there a recommended workflow for setting up these projects manually in STM32CubeIDE?

Thanks in advance for your support and clarification!

Best regards,

1 REPLY 1
CMYL
ST Employee

Hi @jrocher-althea 

I submitted you inquiries internally.

 

Note: just for internal tracking the question reference is Ticket 209175.

 

Best Regards

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.