2020-12-10 2:06 AM
Hi, I am trying activate read protection to level-1 with using batch(.bat) file. I am commanding to ST- Link Utility via batch file. My batch file code is like that:
@ECHO OFF
"C:\Program Files (x86)\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Utility/ST-Link_CLI.exe" -c SWD -OB RDP=0 -ME -P C:\gok.hex -V "after_programming" -OB RDP=1
PAUSE
Explanation of code is;
-c SWD : connects to device
-OB RDP=0 : sets read protection level to 0
-ME: mass erase
-P c:\gok.hex : program hex file to flash
-V "after_programming": verify if programmed correctly
-OB RDP=1 : set read protection to level 1
When I execute batch file it's programming and verifying the selected .hex file and setting read protection to level 1 but my code is not running in the mcu. I tried reseting after executing the batch file but it didn't help. If I erase the "-OB RDP=1" command at the end, code is running.
I have done same things with ST-Link Utility(not with batch file this time- manually), I programmed the hex file and then set the read protection level to 1 and code runned without problem. I can't see what is the difference between my batch file code and doing it manually with ST-Link Utility. I need help at that point.
2020-12-10 5:57 AM
Maybe do it in two separate calls instead of one call. Having two -OB RDP values may be confusing the program.
Could also try with STM32CubeProgrammer CLI. Probably the same result.
2020-12-11 3:10 AM
Thanks for answer. Cube Programmer solved my problem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.