2023-12-20 7:20 PM
Does Secure Manager actually use USART1 when it comes up or is the initial serial output from the default app installed when I provision Secure Manager (SM)?
This output, I mean
================= General Infos ==========================
Flash Layout configuration index: <0x0>
Secure Manager Version: <1.0.0>
STuRoT Version: <1.0.0>
==========================================================
I saw in ROT_Provisioning/SM/Config/SM_Config_General.xml that had elements to change USART and associated GPIOs.
If so, is changing SM_Config_General.xml and re-create the obk enough to change it?
Or, is the SM hardcoded to USART1?
Also does the SM, release or stop using the USART, to allow the non-secure app to use the USART?
We have engineering H573-based boards, in which USART1 was already allocated to another function.
So, would like SM to not use USART1, and if needed, use another USART allocated (temporarily) to a serial console
Solved! Go to Solution.
2023-12-20 11:25 PM
Hello,
this traces are done by a default non secure application that is embedded by default in the full SFI image.
Binary location of this default application ( 2 version depending on the number of ssecure module embedded, default is 0)
STM32Cube_FW_H5_V1.1.1\Projects\STM32H573I-DK\ROT_Provisioning\SM\Binary\appli_0.hex
or
STM32Cube_FW_H5_V1.1.1\Projects\STM32H573I-DK\ROT_Provisioning\SM\Binary\appli_1.hex
We do not provide the source of this basic application.
The SM doesn't produce any traces;-)
The HW resource used by SM is define on this wiki :
https://wiki.st.com/stm32mcu/wiki/Security:SMAK_for_STM32H5
Chapter :
2023-12-20 11:25 PM
Hello,
this traces are done by a default non secure application that is embedded by default in the full SFI image.
Binary location of this default application ( 2 version depending on the number of ssecure module embedded, default is 0)
STM32Cube_FW_H5_V1.1.1\Projects\STM32H573I-DK\ROT_Provisioning\SM\Binary\appli_0.hex
or
STM32Cube_FW_H5_V1.1.1\Projects\STM32H573I-DK\ROT_Provisioning\SM\Binary\appli_1.hex
We do not provide the source of this basic application.
The SM doesn't produce any traces;-)
The HW resource used by SM is define on this wiki :
https://wiki.st.com/stm32mcu/wiki/Security:SMAK_for_STM32H5
Chapter :
2024-01-04 2:43 PM
I didn't see any output from SM, but does SM configure the XML-selected USART anyway?
It seemed I had to do a disable (UE=0) before we could re-configure the USART.
Our USART init code exited when it tested that UE==1 as the first thing upon entry.
Note: we using LL_USART functions instead of HAL_USART functions to keep our code "lean and mean"
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.