2019-04-14 12:03 PM
I have finally managed to get the SBSFU to work on my STM32F4-Discovery board. I've been working on this over the past month until I figured it out and got it to work. For some reason, I couldn't get the 2_Image version to work on my hardware. I believe the FW header was overlapping with one of the Memory Slots' Regions on flash sectors. Will try to get back to this later, however, the 1_Image version worked fine.
Because I wanted to understand the structure of the 3-project based SBSFU lib, I started with new projects from scratch and then added all files, dependencies, IDE configurations, scatter and asm files, and finally modified the .BAT files according to the new location of my projects.
The first two projects worked flawlessly, however, I couldn't imitate the same process for the third project, UserApp, where the customer's firmware merges with the SBSFU core. The project compiles successfully, but the postbuild .BAT script fails to complete the process and no binaries are generated in "Binary" folder. This is only happening in the new project that I have created in a new location. The UserApp project inside the SBSFU demo package compiles and generates the binaries as expected.
I know that the .BAT postbuild script has something to do about it, but no sure what causes the problem as I'm not very familiar with Windows Batch files and their syntax.
The postbuild script throws this error when invoked from within the IDE:
"The syntax of the command is incorrect."
This is also from the output.txt file inside the project:
usage: prepareimage.exe [-h]
{keygen,trans,getpub,sign,sha256,conf,enc,header,pack,merge}
...
prepareimage.exe: error: unrecognized arguments: .\UserApp.bin .\\..\\Binary\\\\UserApp.sfu
"C:\Users\admin\STM32_WS\Middlewares\ST\STM32_Secure_Engine\Utilities\KeysAndImages\\win\\prepareimage\\prepareimage.exe enc -k C:\Users\admin\STM32_WS\CubeMX Generated\STM32F407_SBSFU_UserFW\MDK-ARM\\\..\\..\\SECoreBin\\Binary\\OEM_KEY_COMPANY1_key_AES_CBC.bin -i C:\Users\admin\STM32_WS\CubeMX Generated\STM32F407_SBSFU_UserFW\MDK-ARM\\\..\\..\\SECoreBin\\Binary\\iv.bin .\UserApp.bin .\\..\\Binary\\\\UserApp.sfu > .\output.txt 2>&1 : failed" This is also the postbuild .BAT file after modification:
::Post build for SECBOOT_ECCDSA_WITH_AES128_CBC_SHA256
:: arg1 is the build directory
:: arg2 is the elf file path+name
:: arg3 is the bin file path+name
:: arg4 is the version
:: arg5 when present forces "bigelf" generation
@echo off
set "projectdir=%1"
set "execname=%~n3"
set "elf=%2"
set "bin=%3"
set "version=%4"
set "SBSFUBootLoader=%~d0%~p0\\..\\.."
::The default installation path of the Cube Programmer tool is: "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin"
::If you installed it in another location, please update the %programmertool% variable below accordingly.
set "programmertool="C:\\Program Files\\STMicroelectronics\\STM32Cube\\STM32CubeProgrammer\\bin\\STM32_Programmer_CLI""
set "userAppBinary=%projectdir%\\..\\Binary\\"
set "sfu=%userAppBinary%\\%execname%.sfu"
set "sfb=%userAppBinary%\\%execname%.sfb"
set "sign=%userAppBinary%\\%execname%.sign"
set "headerbin=%userAppBinary%\\%execname%sfuh.bin"
set "bigbinary=%userAppBinary%\\SBSFU_%execname%.bin"
set "elfbackup=%userAppBinary%\\SBSFU_%execname%.elf"
set "iv=%SBSFUBootLoader%\\SECoreBin\\Binary\\iv.bin"
set "oemkey=%SBSFUBootLoader%\\SECoreBin\\Binary\\OEM_KEY_COMPANY1_key_AES_CBC.bin"
set "ecckey=%SBSFUBootLoader%\\SECoreBin\\Binary\\ECCKEY.txt"
set "sbsfuelf=%SBSFUBootLoader%\\SBSFU\\SBSFU.axf"
::comment this line to force python
::python is used if windows executeable not found
pushd %projectdir%\..\..\..\Middlewares\ST\STM32_Secure_Engine\Utilities\KeysAndImages
set basedir=%cd%
popd
goto exe:
goto py:
:exe
::line for window executeable
echo Postbuild with windows executable
set "prepareimage=%basedir%\\win\\prepareimage\\prepareimage.exe"
set "python="
if exist %prepareimage% (
goto postbuild
)
:py
::line for python
echo Postbuild with python script
set "prepareimage=%basedir%\\prepareimage.py"
set "python=python "
:postbuild
::Make sure we have a Binary sub-folder in UserApp folder
if not exist "%userAppBinary%" (
mkdir "%userAppBinary%"
)
::PostBuild is fired if elf has been regenerated from last run, so elf is different from backup elf
if exist %elfbackup% (
fc %elfbackup% %elf% >NUL && (goto nothingtodo) || echo "elf has been modified, processing required"
)
set "command=%python%%prepareimage% enc -k %oemkey% -i %iv% %bin% %sfu% > %projectdir%\output.txt 2>&1"
%command%
IF %ERRORLEVEL% NEQ 0 goto :error
set "command=%python%%prepareimage% sha256 %bin% %sign% >> %projectdir%\output.txt 2>&1"
%command%
IF %ERRORLEVEL% NEQ 0 goto :error
set "command=%python%%prepareimage% pack -k %ecckey% -r 4 -v %version% -i %iv% -f %sfu% -t %sign% %sfb% -o 512 >> %projectdir%\output.txt 2>&1"
%command%
IF %ERRORLEVEL% NEQ 0 goto :error
set "command=%python%%prepareimage% header -k %ecckey% -r 4 -v %version% -i %iv% -f %sfu% -t %sign% -o 512 %headerbin% >> %projectdir%\output.txt 2>&1"
%command%
IF %ERRORLEVEL% NEQ 0 goto :error
set "command=%python%%prepareimage% merge -i %headerbin% -s %sbsfuelf% %elf% %bigbinary% >> %projectdir%\output.txt 2>&1"
%command%
IF %ERRORLEVEL% NEQ 0 goto :error
IF "%~5"=="" goto :finish
echo "Generating the global elf file (SBSFU and userApp)"
echo "Generating the global elf file (SBSFU and userApp)" >> %projectdir%\output.txt
set "command=%programmertool% -ms %elf% %headerbin% %sbsfuelf% >> %projectdir%\output.txt 2>&1"
%command%
IF %ERRORLEVEL% NEQ 0 goto :error
set "command=copy %elf% %elfbackup% >> %projectdir%\output.txt 2>&1"
%command%
IF %ERRORLEVEL% NEQ 0 goto :error
:finish
::backup and clean up the intermediate file
del %sign%
del %sfu%
del %headerbin%
exit 0
:error
echo "%command% : failed" >> %projectdir%\\output.txt
:: remove the elf to force the regeneration
if exist %elf%(
del %elf%
)
if exist %elfbackup%(
del %elfbackup%
)
echo %command% : failed
pause
exit 1
:nothingtodo
exit 0By the way, I have created SBSFU folder in the root directory of the project (where the postbuild script resides) and copied the SBSFU.axf file from the SBSFU project there, and also created SECoreBin/Binary folder and copied all of the ECCKEY, iv.bin, and OEM_Key files inside it as well.
Hopefully someone can help on this!
Thanks
2024-12-25 8:58 AM
Hello @Zaher ,
Thanks for sharing your experience and helping future users with such a task just for notice the .bat script you are using are generated for a python script that you can modify and adapt to your needs.
after giving it a quick look it can be a problem with usage of a mix of absolute and relative paths making it unrecognizable hence the error you are getting. it is good to know that you cannot exceed 256 chars in your path for windows or it can cause problems.
Regards
2024-12-30 6:27 AM
Hello @Zaher ,
did you manage to get the script working?
Regards
2025-01-31 9:57 AM
Hello @STea
Thank you very much for your input. I didn't check my email in a while, so I missed most notifications sent about new posts.
Yes of course, that was done years ago and it's been deployed to hundreds of devices worldwide and still running perfectly. I believe the .bat scripts were wrappers for the python script or something? These were used with the MDK-ARM project, but for Eclipse/GNU-based projects, the scripts are pure python (.py).
Anyways, I'm almost done with a new flavor of the SBSFU tailored to my products and needs. I have made a lot of changes to the state machine, the loader (switched from YMODEM to USB), added product activation, validation with remote server, a GUI utility app, and much more.
Regards,
Zaher
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.