2025-09-29 7:36 AM
Hello!
I am trying to provision a DA certificate on STM32H563 through CANFD Bootloader in system memory.
I am calling special function 0x83 as described in AN2606 and AN5405. As I can understand, this is an RSSLIB_PFUNC->DataProvisioning.
I am filling the structure and place it to the SRAM3. See the picture/hex.
typedef struct {
uint32_t *pSource;
uint32_t *pDestination;
uint32_t Size;
uint32_t DoEncryption;
uint32_t Crc;
} RSSLIB_DataProvisioningConf_t;The structure is placed in 0x2005C000
The 0x60 bytes of the obk payload is placed in 0x2005C000.
The fuction returns Error code 0xF5F58080 (CRC Error).
I've tried several algorythms, byte-reversal, but could not get it worked.
I tried to find an example of using this function, but without success.
So, I am asking for some code example showing this function.
Maybe I need to prepare data somehow. Or add another data in crc calculations.
Thanks!
Solved! Go to Solution.
2025-10-01 6:07 AM
Check the attachment.
This script
After these commands are sent I send folowing slCan sequence to perform a Provisioning:
b05020083
b05020004
b05042005C060
This works for my STM32H563 even in Open product state.
You can port this commands to your CANFD adapter-compatible language.
2025-10-01 6:07 AM
Check the attachment.
This script
After these commands are sent I send folowing slCan sequence to perform a Provisioning:
b05020083
b05020004
b05042005C060
This works for my STM32H563 even in Open product state.
You can port this commands to your CANFD adapter-compatible language.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.