2025-03-17 4:29 PM
Hi,
I have managed to extract the OEMiROT project from H533 into H523 and compiled it successfully using STM32CRYPTO library since H523 does only have limited cryptography accelerator. I have modified the flash_layout.h to match my application (which is only using the non-secure image with no data image). However, the OEMiROT bootloader firmware itself is configured with secure and non-secure parts.
I have been updating the postbuild.sh script to match my project structure. I am at the stage or running AppliCfg.exe and it error out on the flash layout with the following error
[ERR] The script was probably invoked manually with having certain macros nested in flash_layouts.h.
Please revisit the flash_layout.h file and hardcode values for the (NON-)SECURE_IMAGE_OFFSET and (NON-)SECURE_IMAGE_MAX_SIZE macros
I checked these macros and they are matching the ones in map.properties. I also tested with
I attached the following files:
1. flash_layout.h
2. map.properties
3. postbuild.log
Kind Regards,
Hani
Solved! Go to Solution.
2025-03-17 8:45 PM
Hi,
I have fixed the issue. The flash memory layout related macros in the image_macros_processed_bl2.c were not matching the defs in flash_layout.h and thus the script error out. I made sure that the defs in image_macros_processed_bl2.c are compatible with the ones in flash_layout.h
Sorry for raising this issue unnecessarily
Regards,
Hani
2025-03-17 8:45 PM
Hi,
I have fixed the issue. The flash memory layout related macros in the image_macros_processed_bl2.c were not matching the defs in flash_layout.h and thus the script error out. I made sure that the defs in image_macros_processed_bl2.c are compatible with the ones in flash_layout.h
Sorry for raising this issue unnecessarily
Regards,
Hani
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.