2025-04-28 3:11 AM
Hi all,
I am trying to make my NUCLEO N657X0 board working with :
I am having issue in understanding how to get the things done :
I have created a new STM32 project on STM32CubeIDE, ending with having 4 differents projects in the IDE
- AppliNonSecure, AppliSecure, ExtMemLoader, FSBL
I selected generate demo code, and everything works fine in debugging FSBL following the jumpers indications etc...
Until there, no problem.
Now I want to run in the XIP template to execute my code from External Flash.
I found the template STM32Cube_FW_N6_V1.1.0\Projects\NUCLEO-N657X0-Q\Templates\Template_Isolation_XIP
Is there any documentation on how to use this ? There is no STM32CubeIDE project, its just src and inc folders.
Shall I copy paste the source and include files in my previously created projects ?
I am getting a bit lost on how I could start having my NSApp running and start developping my solution.
could you provide any advises ? documentation ?
Kind regards
Thank you very much
2025-05-06 10:41 AM
Hello @jrocher-althea
Your questions are asked internally.
Note: for internal tracking only question reference is 209176
Best Regards
2025-05-13 3:36 AM
Hello @jrocher-althea
Below the answers to your questions. Let me know if this is helpfull.
1) In repository STM32Cube_FW_N6_V1.1.1\Projects\NUCLEO-N657X0-Q\Templates\Template_Isolation_XIP, the template folder contains all project files for EWARM, ARM-MDK and STM32CubeIDE. Check my folder structure in attached picture.
There is also a Readme.html and Readme.md file which are explain how to use it.
2) If Customer has created it's own application using latest STM32CubeMX, the XIP configurations feature can be managed with Middleware EXTMEM_MANAGER in the Boot usecase section and selecting "Selection of the boot system = Execute In Place" where Memory 1 must be XSPI2.
3) You can also refer to STM32Cube_FW_N6_V1.1.1\Documentation\In the STM32CubeN6GettingStarted.pdf the section is 5.1.5 Running the Isolation_XIP (eXecute In Place) template project
Best regards
2025-05-16 3:23 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.