2024-09-03 3:21 AM - edited 2024-09-03 3:30 AM
Hi I am working on SBSFU Application project from STM32U585 project. And I am trying to use mbed-crypto APIs like SHA512 APIs as below
What I am experiencing here is that I am seeing frequent reset of the controller during execution. I would like to know the possibility of same situation ever faced by other person also. Or is their any other configuration I have enable in default config file.
Need help, thanks in advance...
2024-11-28 6:39 AM
Hello @Nitin ,
In which context those calls are used? if it is in the non-secure project context you need to do so with PSA API calls to call for crypto services from secure in a proper way this usecase is implemented in the TFM application example project which can be found under:
STM32Cube_FW_U5_V1.6.0\Projects\B-U585I-IOT02A\Applications\TFM
see TFM\TFM_Appli\NonSecure\Src\tfm_app.c
Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.