2021-08-24 12:03 AM
In SBSFU, bootloader image will be signed?
I am using stm32l562e-dk. I want to use SBSFU.
1) I Have found the SBSFU example for NUCLEO-L552ZE-Q, but I am not able to find it for stm32l562e-dk. Is it available?
2) IN SBSFU when the bootloader is first time flashed, the bootloader's integrity and authenticity are checked?
3) Can i update bootloader in future if i have kept my RDP level to 1?
2021-08-24 11:40 PM
@Frantz LEFRERE Can you please help me regarding this?
2021-08-25 2:06 AM
Its documentation may be found at https://www.st.com/en/embedded-software/x-cube-sbsfu.html#documentation.
It is example software. You should modify or write your own per your requirements.
If your part is not supported, you can only modify or write your own.
In the software, you may encrypt the image payload (your app) or not, and it will sign the image header.
2021-08-25 2:24 AM
>2) IN SBSFU when the bootloader is first time flashed, the bootloader's integrity and authenticity are checked?
No. You need to build and write it to flash properly (that is your integrity). You need to protect it so it cannot be changed without erasing your secret key used for decryption of apps and also used if you are symmetrically signing or your public key if you are asymmetrically signing. You choose how you will protect those, e.g. RDP, PCROP, etc, etc. (that is your authenticity, root of trust).
>3) Can i update bootloader in future if i have kept my RDP level to 1?
If you mean while it is in the field, you would have to implement that, and fear you may have to or have them sent back to your factory for that is the only reason you would ship product with RDP level 1.
During development, yes you can do RDP level 1 to 0 regression per your RM.
You would generally keep all protections disabled during development as having to clear protections before loading code adds to your development time.
2021-08-26 5:03 AM
Please have a look in this MOOC :
1) in the MOOC chapter : TFM implementation on STM32L5
For the STM32L5, the SBSFU doesn't rely on X-SBSFU package but on TFM.
For the Nucleo we deliver a SBSFU ( based on TFM removing all the secure services).
For the DK, a full TFM implementation.
You can easily port the SBSFU implementation from Nucleo to stm32l562e-dk, you just need to adaption the LP_ART/USART for the traces ( optionally you can active the crypto acceleration).
2) for the first flashing you should be in a secure environment to flash it. We also propose mechanism to flash in an unsecure environment called SFI ( Secure Firmware install) .
3) by definition SBSFU should be immutable ( so can't be updated). But if you select only the RDP1 level and the debugging link is still activated, you may do a full RDP regression but this will erase the SBSFU.
2021-08-26 11:56 PM
Thank you so much @Frantz LEFRERE and @alister for your informative answer.
I will try to port SBSFU for DK and let you know if I will have any concerns regarding it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.