2021-04-07 7:20 AM
2021-04-07 9:48 AM
Hello Peter,
I would suggest reusing the fw_update_app.c provided in example application
You can see it is including sfu_fwimg_regions.h which defines these symbols.
Best regards
Jocelyn
2021-04-07 11:44 PM
Hello Jocelyn,
I have reused the UserApp code, but these symbols are defined external in sfu_fwimg_regions.h.
I have scanned the UserApp code but I'm blind to find the definition of these symbols. I need a hint.
The se_interface_app.o lib is included.
Best regards,
Peter
2021-04-08 6:55 AM
the definition should be right underneath the extern declarations but one of these has to be defined (see line 81 in sfu_fwimg_regions.h):
#if defined(SFU_FWIMG_COMMON_C) || defined(SE_LOW_LEVEL_C) || defined(TEST_PROTECTIONS_C)e.g. on line 93:
/* List of slot start address */
const uint32_t SlotStartAdd[NB_SLOTS] = { 0U,
SLOT_ACTIVE_1_START,
SLOT_ACTIVE_2_START,
SLOT_ACTIVE_3_START,
0U,
0U,
0U,
0U,
};where SLOT_ACTIVE_1_START is defined in mapping_export.h
2021-04-08 8:16 AM
That's right, but this block is not active in the UserApp.
I can't find the external definition inside the UserApp project.
Also the three switches are not documented.
2021-04-08 1:09 PM
Hi Peter,
yes this part is not that well documented.
Now, just searching the defines proposed you will see that TEST_PROTECTIONS_C is defined in test_protection.c in the UserApp example.
So, just add this define in your project on you should be fine
Best regards
Jocelyn
2022-01-26 10:42 PM
@Jocelyn RICARD (ST Employee)
Hi Jocelyn,
I am running into a similar problem. I've used the SBSFU UserApp as a base for a new program, and included the same files and copied all project options. My errors are undefined references in my *.o file, for example:
............/src/ota_pal.o:(.rodata.SlotStartAdd+0x4): undefined reference to `__ICFEDIT_SLOT_Active_1_start__'
There are multiple undefined references. The others are:
__ICFEDIT_SLOT_Active_2_start__
__ICFEDIT_SLOT_Active_3_start__
__ICFEDIT_SLOT_Dwl_1_start__
__ICFEDIT_SLOT_Dwl_2_start__
__ICFEDIT_SLOT_Dwl_3_start__
__ICFEDIT_SWAP_start__
__ICFEDIT_SLOT_Active_1_end__
__ICFEDIT_SLOT_Active_2_end__
__ICFEDIT_SLOT_Active_3_end__
__ICFEDIT_SLOT_Dwl_1_end__
__ICFEDIT_SLOT_Dwl_2_end__
__ICFEDIT_SLOT_Dwl_3_end__
__ICFEDIT_SWAP_end__
I can see that these values are present in the UserApp.map file, and are missing in the *.map file of my own application. I do however not know why, as I copied all includes and project setting from the UserApp.
2022-01-27 4:28 AM
Found it,
Forgot the add to the linker script (the *.ld file) the following includes:
INCLUDE mapping_fwimg.ld
INCLUDE mapping_sbsfu.ld
2022-04-11 9:32 AM
@Jocelyn RICARD
My application is also unable to locate SlotStartAdd and SlotEndAdd. I can duplicate the exact behavior I am having with UserApp.
I am unable to explain why adding #define TEST_PROTECTIONS_C to main.c does not cause the app to build.
I have the exact same behavior in my app whose settings closely follow the settings for UserApp.
Could you please help me build my app without having to either comment out most of test_protections or adding a file source file containing only the #define and the two #includes?
2022-04-11 10:22 AM
Not sure if this helps you out, but I do not have a #define TEST_PROTECTIONS_C anywhere in my code. Instead I added it as a define symbol under the project settings in CubeIDE:
settings -> MCU GCC Compiler -> Preprocessor -> Define symbols
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.