2021-07-20 5:18 PM
We were running tests originally with the g474re eval board to test/integrate SBSFU functionality. We needed to disable dual-bank mode with the STM32CubeProgrammer before being able to transfer via Ymodem.
We are now trying on the g491 and are failing this check:
if (SFU_LL_SECU_CheckFlashConfiguration(psFlashOptionBytes) == SFU_SUCCESS)The STM32CubeProgrammer doesn't have the dual bank option for the g491. I'm probably missing something obvious but how can we change dual-bank mode outside of the option bytes page in the programmer? Or is it that it should be enabled and the problem lies in another configuration?
I do have the BFB2 unchecked.
2021-07-21 3:15 AM
>> How to disable stm32g491 dual-bank mode ?
Hello,
I think that G491 is not a dual-bank chip. The DBANK option in STM32CubeProgrammer has been removed since v2.8.0.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.