2023-05-29 10:24 PM
Hi ST Team,
I am using STM32U575 MCU. I want to create signed binary.
I want to upload signed firmware in MCU and also update only new signed firmware via Native bootloader and want to restrict unknown firmware updates.
Can you please guide me.
Thanks in advance,
VIJAY.
Solved! Go to Solution.
2023-06-06 10:36 AM
Hello Vijay,
You will find an example of a secure boot implementing secure firmware update in the STM32CubeFW U5 here:
STM32Cube_FW_U5_V1.2.0\Projects\B-U585I-IOT02A\Applications\SBSFU\
This secureboot is based on open source MCUboot.
ST made an adaptation to STM32U5 to enable hardware secure protections of the device.
It is provided with an example of a secure and non secure applications that will be possibly encrypted and signed. Upon installation, secure boot will check authenticity of the firmware and install it.
What you call native bootloader is probably the bootloader located in system flash allowing download of flashing of firmware in production. This bootloader has no security features implemented, so cannot be used for such purpose.
For your information one of the latest STM32 that is STM32H573 embeds a secureboot in system flash. It is called STiROT for ST immutable Root of Trust.
Best regards
Jocelyn
2023-06-06 10:36 AM
Hello Vijay,
You will find an example of a secure boot implementing secure firmware update in the STM32CubeFW U5 here:
STM32Cube_FW_U5_V1.2.0\Projects\B-U585I-IOT02A\Applications\SBSFU\
This secureboot is based on open source MCUboot.
ST made an adaptation to STM32U5 to enable hardware secure protections of the device.
It is provided with an example of a secure and non secure applications that will be possibly encrypted and signed. Upon installation, secure boot will check authenticity of the firmware and install it.
What you call native bootloader is probably the bootloader located in system flash allowing download of flashing of firmware in production. This bootloader has no security features implemented, so cannot be used for such purpose.
For your information one of the latest STM32 that is STM32H573 embeds a secureboot in system flash. It is called STiROT for ST immutable Root of Trust.
Best regards
Jocelyn
2023-07-06 3:00 AM
Do we have any document which tells how sTirort works , using its STRSS andOB keys.After that how it hand over to OEMirot
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.