2026-03-28 11:00 AM
Hi, I have an STM32H7S78-DK board and am working on encryption. I’ve looked at the example files for STiROT_OEMuROT: https://github.com/STMicroelectronics/STM32CubeH7RS/tree/main/Projects/STM32H7S78 -DK/ROT_Provisioning/STiROT_OEMuROT
I’ve tried that out, and now I’d like to generate my own keys, but what I’m missing are the OEMuROT_Data.obk and STiROT_Data. obk files. I can generate the OEMuROT_Config.obk and STiROT_Config.obk files with their corresponding XML files using STM32TrustedPackageCreator_CLI, but how do I generate the _Data. obk files? They don’t have any config files, and I can’t find anything online either. The batch script uses them, though, as you can see here: https://github.com/STMicroelectronics/STM32CubeH7RS/blob/main/Projects/STM32H7S78-DK/ROT_Provisioning/STiROT_OEMuROT/obkey_provisioning.bat
Please help – do I need them? If so, how are they generated and where can I find the corresponding .xml file?
2026-03-30 10:15 AM
Hello @PaulB_1 ,
the *_data files are “empty” files where payload is composed of zeros.
These files are used to initialise a specific area in OBKey that will be used to store “dynamic” information such as firmware version.
So no need to re generate these files they will not change. This is the reason why xml configuration is not provided
Best regards
Jocelyn
2026-04-04 9:29 AM
Okay, great, thanks for the quick reply. But that means I still have to use the data files. The reason is that I'm writing an API in C# to help with provisioning, and that's why I want to know if I should process the data in the same order as in the batch file.
set "action=Configure OBKeys HDPL1-DA config area"
echo %action%
%stm32programmercli% %connect_no_reset%
%stm32programmercli% %connect_no_reset% -sdp ./../DA/Binary/%da_file%.obk
IF !errorlevel! NEQ 0 goto :error
set "action=Configure OBKeys HDPL1-STiROT config area"
echo %action%
%stm32programmercli% %connect_no_reset%
%stm32programmercli% %connect_no_reset% -sdp ./Binary/STiROT_Config.obk
IF !errorlevel! NEQ 0 goto :error
set "action=Configure OBKeys HDPL1-STiROT data area"
echo %action%
%stm32programmercli% %connect_no_reset%
%stm32programmercli% %connect_no_reset% -sdp ./Binary/STiROT_Data.obk
IF !errorlevel! NEQ 0 goto :error
set "action=Configure OBKeys HDPL2-OEMuROT config area"
echo %action%
%stm32programmercli% %connect_no_reset%
%stm32programmercli% %connect_no_reset% -sdp ./Binary/OEMuROT_Config.obk
IF !errorlevel! NEQ 0 goto :error
set "action=Configure OBKeys HDPL2-OEMuROT data area"
echo %action%
%stm32programmercli% %connect_no_reset%
%stm32programmercli% %connect_no_reset% -sdp ./Binary/OEMuROT_Data.obk
IF !errorlevel! NEQ 0 goto :error
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.