2020-12-22 5:31 PM
2020-12-23 3:29 AM
Hello @JBuse.1 ,
Welcome to the STM32 Community :smiling_face_with_smiling_eyes:
Our HAL provided examples, based on either cryptolib or HW accelerators, are validated with NIST vector matching.
The processed results are always compared to expected ones from NIST test suits.
Hope this answer your question.
Otherswise, please share more details: which family, HAL examples, versions ?
Imen
2020-12-23 8:20 AM
Hello Imen,
First thank you for the very quick reply.
I am trying to get the HAL_CRYP_Decrypt() or HAL_CRYP_Encrypt() method to produce results that match the below NIST test vector, and I cannot seem to get it to match. I use the following settings:
Crypto::hcryp.Instance = CRYP;
Crypto::hcryp.Init.DataType = CRYP_DATATYPE_8B;
Crypto::hcryp.Init.KeySize = CRYP_KEYSIZE_128B;
Crypto::hcryp.Init.Algorithm = CRYP_AES_GCM;
Crypto::hcryp.Init.Header = (uint32_t *)NULL;
Crypto::hcryp.Init.HeaderSize = 0;
Crypto::hcryp.Init.KeyIVConfigSkip = CRYP_KEYIVCONFIG_ONCE;
Crypto::hcryp.Init.DataWidthUnit = CRYP_DATAWIDTHUNIT_WORD;
Crypto::hcryp.Init.pKey = (puint32_t)key_;
Crypto::hcryp.Init.pInitVect=(puint32_t)iv_;
The test vector is line 4417 of the gcmDecrypt128.rsp file. I have validated this test vector with the STM32H7's AES ECB encrypt functionality and a software GCM implementation. I have checked your example projects, and there are AESGCM examples but they do not generate a NIST approved vector for verification.
[Keylen = 128]
[IVlen = 96]
[PTlen = 128]
[AADlen = 0]
[Taglen = 128]
Count = 0
Key = e98b72a9881a84ca6b76e0f43e68647a
IV = 8b23299fde174053f3d652ba
CT = 5a3c1cf1985dbb8bed818036fdd5ab42
AAD =
Tag = 23c7ab0f952b7091cd324835043b5eb5
PT = 28286a321293253c3e0aa2704a278032
Any help would be appreciated. Thank you,
Jon
2020-12-24 12:24 AM
Please check the STM32H7 series used and its compatibility with the appropriate Cryptolib version as below (or X-CUBE-CRYPTOLIB Data briefDB2660 - Rev 5 - November 2020 for all series compatibility)
Imen
2020-12-28 8:10 AM
Hi @JBuse.1 ,
Please mark my answer as best by clicking on the "Select as Best" button if it fully solved your issue. This will help other users find this solution more quickly.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.