2022-10-12 1:14 AM
Hello,
I wanted to try the SBSFU topic 6 step by step youtube video, i accidentally flash the Userapp.bin with the RDP level 1, (and also with Write protection enable in bank1).
I try to change the RDP level back to 0, and also disable the Write protection on bank1, however the mass erase option had not been successful, can you advise if such revert is possible? it means that those protected area was not able to be erase.(0x8000000), or the board had become unusable?
Solved! Go to Solution.
2022-10-17 4:04 AM
Hello @digidhamu ,
the reset pin should be connected to the STLink so that it can handle it.
This is the purpose of connect under reset.
STLink maintains reset enabled, requests connection to jtag and releases the reset.
You can connect when setting boot0 to VCC because this connection does not require connect under reset.
Best regards
Jocelyn
2022-10-17 4:13 AM
Great @Jocelyn RICARD This works perfectly. Thanks for your timely support.
2023-03-01 1:55 AM
It was possible to unbrick my G071 bij using the old and better tool: STM32 ST-LINK Utility 4.4.0.0
This tool is more clear. On the tab Option Bytes > Read/Write Protection (PCROP) the protection on area 1 was enabled.
In cubeprogrammer i did not see this being set.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.