2021-11-02 7:14 AM
Hello,
with a new never programmed stm32g031 chip I get different values for PCROP if the same chip is read with ST-LINK or with bootloader+UART.
The CubeProgrammer version is 2.7.0
Which is the reason for that?
Thank you
2021-11-02 7:21 AM
Do you use recent versions of both programs? Do both programs support the stm32g031?
2021-11-02 7:54 AM
The program used is the same, CubeProgrammer version 2.7.0, and run in the same Linux PC.
The most recent version available is 2.8.1
I can give it a try.
The chip is detected and others operation like programming o reading flash are ok.
2021-11-02 1:42 PM
Upgraded to 2.8.1 but the problem is still there
2021-11-17 7:35 AM
Hi @S-.1 ,
I confirm, the PCROP values displayed in ST-Link and the bootloader are different, but it's just the display that differs (one shows the start address of the sector and the other the end address ) .I want to highlight that both are handled correctly by CubeProgrammer.
I will submit a ticket internally to harmonize the display in future version of STM32CubeProgrammer.
Hope this helps you, if your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Houda
2021-11-22 9:42 AM
Hi @Houda Ghabri
Using the ST bootloader only region 1A is shown. Reading data using st-link the regions shown are two: 1A and 1B
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.