2021-05-17 8:53 PM
Currently working on a Bitcoin hardware wallet on the STM32F7 Discovery platform. I wanted to use the cryptographic library to secure information stored in the EEPROM as well as perform hashing functions.
VFP is not supported in libSTM32CryptographicV3.0.0_CM7_GCC_ot.a
Is there anybody that works at STM that would compile an object file with GCC and DM me with a copy.
Where:
Floating-point unit = 'FPv5-SP-D16'
Floating-point ABI = 'Hardware implementation (-mfloat-abi=hard)'
Mcu = 'STM32F746NGHx'
Board = 'STM32F746G-DISCO'
I have seen this done before here...
https://community.st.com/s/question/0D50X00009Xke2s/xcubecrypto-library-cubemx-help
by STOne-32
Thanks Russeree
Solved! Go to Solution.
2021-05-17 9:33 PM
Found the solution for F7 users.
Download patch 3.1.3 for the crypto lib and use the libraries for the H7 series chip.
The lib you are looking for is 'STM32CryptographicV3.1.3_CM7_GCC_ot_fpu.a'
2021-05-17 9:33 PM
Found the solution for F7 users.
Download patch 3.1.3 for the crypto lib and use the libraries for the H7 series chip.
The lib you are looking for is 'STM32CryptographicV3.1.3_CM7_GCC_ot_fpu.a'
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.