cancel
Showing results for 
Search instead for 
Did you mean: 

AES key storage in STM32WL33CCV6 and STM32WBA50KG

SamC
Associate II

Hello,

I will use the STM32WL33CCV6 as a wM-Bus gateway and the STM32WBA50KG for BLE 5.4 communications.

We will encrypt these links with AES key.

1) For STM32WL33CCV6 and wM-Bus, AES-128-CBC and eventually CMAC authentification will be used. It will be static or dynamic symmetric keys.

--> Is it possible to store the keys in the STM32WL33CCV6 MCU ? we want to be secure, especially to respond to the RED 2. 

--> If yes, is it possible to store several keys ?

--> If yes, in the case of dynamic key use, is it possible to update the keys ?

 

2) For STM32WBA50KG and BLE, AES-128 or 256 bits will be used.

--> To respond to the RED 2 AES128 is sufficient or AES-256 is needed ?

--> Compared to the STM32WL33CCV6, I think it's possible to store the key in the MCU, it seems to be a dedicated secure key storage, can you confirm ?

 

Best Regards,

 

1 REPLY 1
CMYL
ST Employee

Hi @SamC 

I shared your question internally with experts and asked for the best key management way.

I let you know when any feedback is received ( Ticket 205144, not usefull for you, this is for me to follow up the internal support)

 

Best regards,

Younes

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.