2012-05-15 5:39 AM
Has somebody tried to port a Z80 emulator to a Cortex M3/M4 device ?
I'm experimenting with the emulator core as found there:http://
My preferred host is this:http://
I'm quite sure that M3 devices with sufficient controller performance are available. A full CP/M simulation is out of scope at the moment (mostly because of time...). The target(s) I have in mind feature 4...20kB ROM and 16..32k RAM, and have a smaller, ROM based ''OS'', actually more a simple program loader than an OS. A CP/M emulation (64k RAM) would hardly be possible with a M3 without external RAM. The host (stm32-lcd) has a display and mass storage, and at least the possibility to add external RAM to emulate the full 64k address range of the Z80.2015-08-25 3:37 PM
If you have a web page, it would be of general interest.
2015-08-26 6:58 AM
Sorry, no Web page. I suppose I could create one but I'd rather not. Now that there is some interest I will need some time to clean up the source as well as verify that there are no copyright violations.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.