2017-07-24 4:38 AM
Hello
i use stm32f103c8 and use this library
.it work without any problem in all pin(16 pin) of gpio.but it work on only one of the port (gpioa-gpiob) and i can olny use one of the port and 16 out put but i need 32 output.how can use two port at the same time?2017-07-24 4:49 AM
You can't. Use a second timer with suitable DMA channels.
JW
2017-07-24 7:13 AM
Asked and Answered
https://community.st.com/0D50X00009XkXm1SAF
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.