2012-04-13 4:24 PM
Hello, for months I've been trying to compile working code for my (generic) STM32 development board with the GCC toolchain, sadly with no success.
Does anyone have/know of a example of a simple project ie. blink an LED, on the web with makefile/linker script/etc. that I could potentially use to get started developing for the STM32 ? Thanks ! - postheavily
edited 4/14/2012 at 9:31am EST2012-04-14 6:00 AM
You could try this:
http://
It works (at least, it worked for me; I could build and debug a simple example). However, they obviously took header files and linkerscript from the Atollic toolchain.2012-04-14 4:32 PM
Hi,
Sorry about the lack of success! Maybe my story will help. Using WinXP and Win7.I started with the Raisonanse RIDE development environment which uses GCC as it's backend - which worked fine for compiling STM32 applications. I wanted to move away from the IDE to makefiles (and also to C++), so downloaded the Yagarto port of GCC and tools. I could not get code to run when compiled under Yagarto. The source was identical, but I suspect that the Yagarto was pulling in some non-thumb code. So, my current compile environment is the Yagarto tools (make, rm, cp, touch) combined with the Raisonance port of the GCC compiler, with all compilation managed using makefiles. There where further complications to get C++ working, but that is another story.Best wishes,Carl.2012-04-15 8:38 AM
Look at this: http://www.freddiechopin.info/en/download/category/6-examples
2012-04-15 7:50 PM
I've had no problems with Yagarto (under WinXP):
There are many example projects as well there, including ones for STM32.2012-04-16 4:57 AM
Of the ''free'' tools I've played with for STM32 Coocox is the only one I'd recomend. For an IDE based on eclipse they've done a really good job.
www.coocox.org For my professional work I use a bought in tool chain (Crossworks) as so called ''free'' tools can be expensive if you value your time.2012-04-16 6:03 AM
The CoIDE (and the rest of the CooCox tools) is Windows-only, which might not be an hindrance.
The CoIDE is more targeted to beginners - this is especially obvious in the debug options and settings, which are very limited, compared other IDEs. If you don't need the yet quite experimental M4 support, it works well. Some other controllers and debug adapters are supported, but the list appears somehow random. The CooCox RTOS also seems to be in an experimental stage - it fails with optimization level > 0. But generally, it is worth a try.2012-04-21 1:58 AM
2012-04-29 4:08 PM
I realize this thread is getting a little stale; I doubt it will help the O.P., but I put a couple of minimal Makefile examples (with minimal instructions) at
By the way those are some excellent links Gloryman. Thanks!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.