2018-03-10 8:45 AM
Hi,
I just purchased the following setup:
Computer: i7 / Windows 10
Nucleo: STM32F401
Expansion: IDW04A1
I have Trustudio as the compiler currently. Updated drivers to current.
My problem is that when working the hands-on tutorial I can not get past the VCOM example.
I drop the Project.bin into the Nucleo board per the instructions open a terminal window and get only garbage output from the Wifi module. The blue LED2 is flashing and the others are solid (LED1 and LED4).
I am stuck and not sure how to proceed if I can't get the module to work with this simple example.
Thank you in advance for any insights here.
Drake
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.