2021-02-02 7:51 AM
I am doing one project with STM32H743ZI.
I am using the external interrupt and copy the signal and set the output as input.
But is shows about 700us delay.
I do not know the reason why its gives such a big delay.
2021-02-02 8:47 AM
There is something wrong. Recheck your setup. Test on another board, etc.
2021-02-02 8:56 AM
What frequency is the signal?
Illustrate with a small/tight code example.
Perhaps Wire or Gates might be more suitable?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.