2024-02-01 12:54 AM - edited 2024-02-01 3:17 PM
I am testing the initialization module.
The issue is that while debugging, when I set a break point in the if statement or use the printf statement above the while in the sample below, it hangs.
It seems to be an event related issue, is there any way to handle this?
In particular, if I use a lot of printf statements, I get hung.
device : STM32F103xE
debugger(driver) : j-link
IICcnt = 0;
while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_RECEIVED))
{
if( IICcnt > IICMAXDELAY ) // breakpoint to here.
{
/* Send STOP condition */
I2C_GenerateSTOP(I2C1, ENABLE);
/* Clear EV6 by setting again the PE bit */
I2C_Cmd(I2C1, DISABLE);
ret = ERROR_I2C_READDATA_RDDATA;
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.