2020-07-08 12:29 PM
I'm trying to test the window watchdog timer but when I'm calling HAL_WWDG_Init(), it redirects to reset handler and whole system restarts. Below is my code, I'm showing here only important lines.
/******************************************/
WWDG_HandleTypeDef hWWDG; // In the global
int main()
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_WWDG_Init();
HAL_Delay(20);
HAL_WWDG_Refresh(&hWWDG);
if( __HAL_RCC_GET_FLAG(RCC_FLAG_WWDGRST) == SET)
{
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
__HAL_RCC_CLEAR_RESET_FLAGS();
}
else
{
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
}
while (1)
{
// HAL_WWDG_Refresh(&hWWDG);
HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_12);
HAL_Delay(42);
HAL_WWDG_Refresh(&hWWDG);
}
}
}Below is the code for clock initialization
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;
__PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = 16;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
HAL_RCC_OscConfig(&RCC_OscInitStruct);
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK |
RCC_CLOCKTYPE_PCLK1 |RCC_CLOCKTYPE_PCLK2 | RCC_CLOCKTYPE_SYSCLK;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2);
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
HAL_NVIC_SetPriority(SysTick_IRQn,0,0);
}window watchdog initialization code
static void MX_WWDG_Init(void)
{
__HAL_RCC_WWDG_CLK_ENABLE();
WWDG_InitTypeDef WWDG_InitStruct;
hWWDG.Instance = WWDG;
WWDG_InitStruct.Prescaler = WWDG_PRESCALER_8;
WWDG_InitStruct.Window = 80;
WWDG_InitStruct.Counter = 127;
WWDG_InitStruct.EWIMode = WWDG_EWI_ENABLE;
__HAL_WWDG_ENABLE(&hWWDG);
if(HAL_WWDG_Init(&hWWDG) == HAL_OK)
{
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);
}else
{
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);
}
}can someone suggest what is the cause for getting reset. Don't look at values for counter and window they are randomly taken.
2020-07-08 12:47 PM
If you enable the WWDG while the counter is outside the window you'll force a watchdog reset. You can't use random numbers for window and counter. The counter must be larger than the lower window at 0x40 and less than the upper window value. Either an early or late counter load causes a reset.
Jack Peacock
2020-07-08 2:24 PM
I removed HAL_WWDG_ENABLE() macro but still it causing reset while calling HAL_WWDG_Init(&hWWDG) function. once initialization done I can think about the delays. counter and window are taken from example there it used to work but in this board I've not tested that's why I called it as random. But I think the main problem is initialization. Can you be more specific what else should I do?
2020-07-08 6:08 PM
Always include your chip part number in your post.
2020-07-08 6:15 PM
hWWDG.Instance = WWDG;
WWDG_InitStruct.Prescaler = WWDG_PRESCALER_8;
WWDG_InitStruct.Window = 80;
WWDG_InitStruct.Counter = 127;
WWDG_InitStruct.EWIMode = WWDG_EWI_ENABLE;
__HAL_WWDG_ENABLE(&hWWDG);
if(HAL_WWDG_Init(&hWWDG) == HAL_OK)the top line assigns to hWWDG. The other lines assign to WWDG_InitStruct.
Then you enable it without initializing first.
Then you call initialization on hWWDG, which doesn't use any of the values you've assigned to WWDG_InitStruct.
So, multiple issues.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.