2017-07-18 4:51 AM
Workalot would like to obtain the MCU's ID, just like the STM32 ST-Link utility does. It reports an ID 0x413 and a 1MB Flash for my STM32F4Discovery.
To be clear, I am not after the 96 bit UID (at 0x1FFF7A10) nor am I looking for the SCB.CPUID (ARM CPU).
Such details surely reside in the MCU's ROM memory space. I look at documentation but I must looking in the wrong places.
thank you and regards,
2017-07-18 5:02 AM
It's in the DBGMCU_IDCODE register. check the reference manual for your chip.
uint8_t len = 0;
char devidString[128] = {0}; uint32_t idcode = DBGMCU->IDCODE & 0xFFF; switch (idcode) { case 0x410: len += sprintf(devidString+len, 'stm32f1xx medium-density'); break; case 0x411: len += sprintf(devidString+len, 'stm32f2xx'); break; case 0x412: len += sprintf(devidString+len, 'stm32f1xx low-density'); break; case 0x413: len += sprintf(devidString+len, 'stm32f405/407xx and stm32f415/417xx'); break; case 0x414: len += sprintf(devidString+len, 'stm32f1xx high-density'); break; case 0x415: len += sprintf(devidString+len, 'stm32l4xx'); break; case 0x416: len += sprintf(devidString+len, 'stm32l1xx medium-density'); break; case 0x417: len += sprintf(devidString+len, 'stm32l0xx'); break; case 0x418: len += sprintf(devidString+len, 'stm32f1xx connectivity line'); break; case 0x419: len += sprintf(devidString+len, 'stm32f4xx high-density'); break; case 0x420: len += sprintf(devidString+len, 'stm32f1xx value line'); break; case 0x421: len += sprintf(devidString+len, 'stm32f446xx'); break; case 0x422: len += sprintf(devidString+len, 'stm32f3xx'); break; case 0x423: len += sprintf(devidString+len, 'stm32f4xx low power'); break; case 0x425: len += sprintf(devidString+len, 'stm32l0xx cat. 2'); break; case 0x427: len += sprintf(devidString+len, 'stm32l1xx medium-density/plus'); break; case 0x428: len += sprintf(devidString+len, 'stm32f1xx value line high-density'); break; case 0x429: len += sprintf(devidString+len, 'stm32l1xx cat. 2'); break; case 0x430: len += sprintf(devidString+len, 'stm32f1xx xl-density'); break; case 0x431: len += sprintf(devidString+len, 'stm32f411re'); break; case 0x432: len += sprintf(devidString+len, 'stm32f37x'); break; case 0x433: len += sprintf(devidString+len, 'stm32f4xx de'); break; case 0x434: len += sprintf(devidString+len, 'stm32f4xx dsi'); break; case 0x435: len += sprintf(devidString+len, 'stm32l43x'); break; case 0x436: len += sprintf(devidString+len, 'stm32l1xx high-density'); break; case 0x437: len += sprintf(devidString+len, 'stm32l152re'); break; case 0x438: len += sprintf(devidString+len, 'stm32f334'); break; case 0x439: len += sprintf(devidString+len, 'stm32f3xx small'); break; case 0x440: len += sprintf(devidString+len, 'stm32f0xx'); break; case 0x441: len += sprintf(devidString+len, 'stm32f412'); break; case 0x442: len += sprintf(devidString+len, 'stm32f09x'); break; case 0x444: len += sprintf(devidString+len, 'stm32f0xx small'); break; case 0x445: len += sprintf(devidString+len, 'stm32f04x'); break; case 0x446: len += sprintf(devidString+len, 'stm32f303 high-density'); break; case 0x447: len += sprintf(devidString+len, 'stm32l0xx cat. 5'); break; case 0x448: len += sprintf(devidString+len, 'stm32f0xx can'); break; case 0x449: len += sprintf(devidString+len, 'stm32f74xxx/stm32f75xxx'); break; case 0x450: len += sprintf(devidString+len, 'stm32h7xxx'); break; case 0x451: len += sprintf(devidString+len, 'stm32f76xxx/stm32f77xxx'); break; case 0x452: len += sprintf(devidString+len, 'stm32f72xxx/stm32f73xxx'); break; case 0x457: len += sprintf(devidString+len, 'stm32l011'); break; case 0x458: len += sprintf(devidString+len, 'stm32f410'); break; case 0x463: len += sprintf(devidString+len, 'stm32f413'); break; default: len += sprintf(devidString+len, 'unknown device\r\n'); }uint32_t revCode = (DBGMCU->IDCODE & DBGMCU_IDCODE_REV_ID_Msk) >> DBGMCU_IDCODE_REV_ID_Pos;
switch (revCode) { case 0x1000: len += sprintf(devidString+len, ' Revision A\r\n'); break; case 0x1001: len += sprintf(devidString+len, ' Revision Z\r\n'); break; }/*
For example, it is read as RevA -> 0x1000, Cat 2 revZ -> 0x1001, rev1 -> 0x1003, rev2 ->0x1007, revY -> 0x100F for STM32F405/407xx and STM32F415/417xx devices
For example, it is read as RevA -> 0x1000, Cat 2 revY -> 0x1003, rev1 -> 0x1007, rev3 ->0x2001 for STM32F42xxx and STM32F43xxx devices For example, it is read as RevZ -> 0x1000, Cat 2 revA -> 0x1001 for STM32F401xB/C devices For example, it is read as RevA -> 0x1000, Cat 2 revZ -> 0x1001 for STM32F401xD/E devices For example, it is read as RevA -> 0x1000 for STM32F411xx,STM32F413/423xx,STM32F469/423xx, STM32F446xx and STM32F410xx devices For example, it is read as RevZ -> 0x1001, Cat 2 revB -> 0x2000, revC -> 0x3000 for STM32F412xx devices*/
printf('%s', devidString);
2017-07-18 5:05 AM
Hello,
Look at your reference manual RM0090 in ( 38.6.1 MCU device ID code )
Regards
Imen
2017-07-18 8:14 AM
DBGMCU_IDCODE
0xE0042000
Use it here in system_stm32f4xx.c to detect the specific part and set clocks/plls optimally.
2017-07-18 1:47 PM
Yes, I knew it had to be a simple thing. Thank you all for your promptness and accuracy.
Regards, Workaot
2017-07-18 4:39 PM
>It reports an ID 0x413 and a 1MB Flash for my STM32F4Discovery.
You can determine the flash size by reading FLASHSIZE_BASE register which is defined in STM32Cube_FW_F4_V1.16.0/Drivers/CMSIS/Device/ST/STM32F4xx/Include/stm32f407xx.h
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.