2015-07-05 11:32 PM
Hi guys,
I have been programming with Arduino, however, it seems that I need something more powerful. So I started doing some research and I am particularly interested in STM32. The problem is, the learning curve is extremely steep, as I do not have any experience in embedded programming. I have found a book called ''Discovering the STM32 Microcontroller'' which is based on STM32F100. How different is a F100 to a F103? Will I be able to code the F103 if I follow this book? Lastly, where is a good place to start for a beginner with no experience in embedded programming? Thank you in advance.2015-07-06 1:59 AM
Hello,
1) How different is a F100 to a F103? • 100 or 103 is the Device subfamily: for more information about Part numbering, you can check, the section ordering information scheme in STM32 datasheets• The reference manual to be used for STM32F100 devices is RM041, while the one to get as reference for STM32F103 is RM0008.2) Where do I start learning STM32?This link is about STM32F1 products where you can find documentation: reference manuals, datasheets, and errata sheets: 3) Also I would suggest you to download free software example from cube package STM32cubeF1 available via this link: as beginning to develop your own solution using the STM32F1 product.I hope this answered your questions.Syrine2015-07-06 5:27 AM
Thank you for your answer.
I had a look at all these documents. However, they do not really make sense to me. It's extremely confusing. Also there are numerous documents and I don't know which one to even start with. Is there a more beginner friendly way to start programming STM32?2015-07-06 6:35 AM
I've found the ability to read technical documentation is a key skill. Being strongly proficient in C on a non-embedded platform will also help. At the very least scan the available documentation so you know where the information is located and you can cross-reference it quickly if needed.
The F100 book should be fine for the F103, the F100 was on the VL-Discovery board and has a subset of the function of the F103 parts. Joseph Yiu's Cortex-Mx books are also a good source of information, though not STM32 specific. The peripherals around the ARM core are vendor specific, but typically very similar funcitonality.2015-07-06 12:57 PM
Don't expect too much help from the IC vendors. They sell to professional engineers working on commercial projects. This is a fairly advanced environment that assumes one has several years experience in embedded design, both programming and electronics. IC vendors don't have the resources to teach introductory programming and electronics; that's what schools are for.
Your best approach may be to find an active hobby community for a board (like the Arduino) and start learning with the products the community offers. You might try looking at the ''Netduino'' project. I haven't used it but it seems to be an upgrade path from Arduino to STM32F4 and Cortex M controllers. You might also look at the Spark-Fun website (disclaimer, haven't seen it for some time but it used to have a lot of starter projects). Jack PeacockWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.